Other Parts Discussed in Thread: SN6501, ISO1412, ISOW7841, THVD1500
Hi,
As I was suggested SN65HVD7x series RS-485 Transceivers for the Full-Duplex, I would like to know the working of integrated Enable pins as well as Does TI offers any Integrated Isolators with RS-485 Transceivers?
Looking at the SN65HVD7x series RS-485 Transceivers it can be seen that it supports either Driver and Receiver enable OR Without those enable(Integrated).
Which one do you suggest to go with?
Could you please elaborate on the Integrated Enable use case? (Less pin count?) as well in case of integrated Enable on Driver will be always pulled to high and receiver enable is pulled low ? .
Are there any Integrated Isolators Transceivers like ADM2582E (Full-Duplex).
Also may I know the use of Level shifter(SN74LV1T34DBVR) with Transceivers as in the reference design of

Thank you.