Part Number: TUSB8041
Hi Team,
We developed the system having TUSB8041 before and the device worked as USB2.0.
Recently, new project was kicked off and we wanted to reuse the circuit but we faced following issue.
[Issue]
When connecting two high data rate devices to the hub such as USB camera, one USB device was stuck.
[Our guess]
We are guessing this issue is caused by a band shortage due to large traffic of the cameras.
[Questions]
Then I have two questions to solve this issue.
1. Is this HW issue or SW issue?
2. If this is HW issue, How much data rate USB devices can we connect to TUSB8041 safely?
It's nice if you can advice me how to evaluate the system to eliminate this issue.
Regards,
Takashi Onawa