This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CP22: Selection of Tantalum Electrolytic Cap

Part Number: DS90CP22


The datasheet for this part recommends using both external bypass caps of the RF ceramic type and the tantalum electrolytic type. It does not recommend a range of values for the tantalum electrolytic cap. Is there a guideline on how we would select which value to use in our design? 

Our application is using this IC in both the 1:2 splitter and 2:1 MUX configurations. The LVDS signals we are using have a variable data rate from 2Mbps to 400Mbps.