Part Number: THVD1450
Hi Team,
My customer has a question on the behavior of the enable time for the THVD1450.
It's our understanding that we can tie the drive enable and receive enable pins together and drive them from a single logic signal. But looking at the switching characteristics in section 7.8, and when you put it all together it seems like, if you use this part in half-duplex mode like this, it takes from 2.5-10 microseconds to switch into drive mode, and 4-14 to switch back into receive mode. But if you for some reason are enabling both at once, it only takes the entirely reasonable 100ns or less.
Can you help us understand if we are interpreting this correctly? It seems like the delay to get data around a multidrop system is way too high.
Thanks,
Mitchell