This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CF384AQ-Q1: Looking for 1.8V LVDS to 3.3V TTL RGB bridge IC?

Part Number: DS90CF384AQ-Q1


Hi Sir,

My customer is looking for a solution which can support input 1.8V LVDS  and output 3.3V TTL RGB bridge IC,

Is DS90CF384AQ-Q1 suitable for them? If not, pleas suggestion the right solution.

The topology as below

MTK MT2712C (LVDS) --> Bridge IC (DS90CF384AQ-Q1)--> 3.3V TTL RGB (800 x 480) display

If we don't have right solution for LVDS to RGB, do we have one chip solution for MIPI-DSI to RGB?

Because MTK MT2712C can config to LVDS or MIPI-DSI output. so if we have MIPI-DSI to RGB bridge IC, it is also good for my customer.

Please advice.

Thank you