Part Number: TUSB1064
Hello ,
I use TUSB1064 to transmit DP and USB3.0 signals on the TYPE-C interface. How can I adjust the EQ value to achieve the best signal, can I provide the reference setting method and value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB1064
Hello ,
I use TUSB1064 to transmit DP and USB3.0 signals on the TYPE-C interface. How can I adjust the EQ value to achieve the best signal, can I provide the reference setting method and value?
Peggie
SSEQ EQ tuning will be based on USB TX electrical compliance test. You wand to find the best SSEQ setting that will pass the USB TX electrical compliance test.
DPEQ and EQ tuning will be based on DP/USB RX Jitter tolerance compliance test.
You can also tune SSEQ, EQ, and DPEQ based on the USB/DP functional result if TX/RX electrical compliance is not available.
Thanks
David