Part Number: TCA9509
Hello,
Is there a protection diode connecting SCL(SDA) pin with Vcc pin in TCA9509?
(SCLA pin - VCCA pin,
SDAA pin - VCCA pin,
SCLB pin - VCCB pin,
SDAB pin - VCCB pin)
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9509
Hello,
Is there a protection diode connecting SCL(SDA) pin with Vcc pin in TCA9509?
(SCLA pin - VCCA pin,
SDAA pin - VCCA pin,
SCLB pin - VCCB pin,
SDAB pin - VCCB pin)
Thanks.
Hello,
No, these pins only have protection diodes that are referenced to ground. (You can see this to some extent in the Absolute Maximum specifications table - the maximum input voltage is fixed at 6 V rather than being a function of VCC.)
Regards,
Max