Part Number: TLK2711-SP
Hi,
In the datasheet for pin ENABLE (and some others) it is written that it has internal pullup of 10K (page 5 note 1), but in the Iil (Current input Low) parameter in the TTL Input Electrical Characteristics chapter 7.5 table, it is written that if the input pin is 0.4V the current is -40uA . it is not make sense because if there is internal pull up of 10K the current should be about (2.7-0.4)/10K=0.23mA.
what I am missing here?