Part Number: TUSB3410
Hi Sir,
Customer got the image from our datasheet that the 22pF not placed on the USB bus between 33ohm and resistor and TUSB3410, it requires extra nets from Caps to TUSB3410. Is it any special requirement for this layout method? If, so could you share me why we suggest customer to follow this way?
BTW, if the caps can be un-mounted... could they do the weir directly from USB bus 33ohm to TUSB3410?
Thanks,
George