Part Number: TPS65983B
I have a customer working on a Thunderbolt 3 (TBT3) solution based on Intel's Apex Creek design.
They were able to interface one of their PCIe add-on boards to a TBT3 port on a laptop.
They've since modified the design, removing the PP_EXT circuit. After this change, they are having issues with RESETZ not being released as expected.
They must do the following to release RESETZ properly:
- Power off our circuit board and the laptop
- Make sure the TBT3 cable is disconnected from our circuit
- Power on the laptop and our circuit board
- Plug the TBT3 cable into our circuit board
Once this is done, RESETZ is released and everything works fine.
Customer suspects there is a firmware issue in which firmware is setup to use PP_Ext power for VBUS.
Can you comment?