Part Number: TRS3253E
Hi,
As per table in datasheet (Vcc vs cap values), Can customer use C2, C3 and C4 as 0.47uF and C1 as 0.1uF. Will this affect the operation? Operating voltage (VCC) is 5V.
Thanks,
Akshat
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TRS3253E
Hi,
As per table in datasheet (Vcc vs cap values), Can customer use C2, C3 and C4 as 0.47uF and C1 as 0.1uF. Will this affect the operation? Operating voltage (VCC) is 5V.
Thanks,
Akshat
Hi Akshat,
These values are fine to use and align with the datasheet recommendations.
To get a better understanding of the charge pump operation in these devices and how different capacitor values impact operation, you may want to reference this blog:
If you have any further questions please let us know.
Regards,
Max
Hi Max,
In the datasheet, given Vcc values are 3.3V, 5V and '3V to 5.5V'. For '3V to 5.5V' the given cap values are C1 = 0.1uF, C2, C3 and C4 = 0.47uF.
In our design Vcc is 5V and used cap values are 0.047uF and 0.33uF for C1 and C2,C3 & C4 respectively. But due to cap unavailability in X7R value, we need to change cap value but need to maintain 5V Vcc. So can I use the cap values 'C1 = 0.1uF, C2, C3 and C4 = 0.47uF' for which Vcc range is '3V to 5.5V'?
Can you give more info on Vcc range '3V to 5.5V'? Datasheet had not mentioned much about this option.
Regards,
Gurudev H P
| Review |
| Anole-D ESD report |
Gurudev,
You're right. The config 'C1 = 0.1uF, C2, C3 and C4 = 0.47uF' can cover both 3.3V and 5V supplies. If your supply is 5V only, you have option to choose either 'C1 = 0.047uF, C2, C3 and C4 = 0.33uF' or 'C1 = 0.1uF, C2, C3 and C4 = 0.47uF'. If some cap values are not available, you could try to make C1/C3 ratio close to 0.0047/0.33 or 0.1/0.47, while keeping C2=C4. I hope this makes sense to you.
Regards,
Hao