Part Number: SN65HVD1176
Hello,
I'm trying to do the "Input voltage ranges" test specified in TIA-485-A. Therefore, I have to apply -7V to terminal A and -6.8V to terminal B of the transceiver (see Table 1 in section 4.3.2 of the standard). During the test the transceiver is on but the driver is disabled.
When I switch the power supplies on they ramp with approx. 70mV/us to the specified values, the transceiver is destroyed and I have a short circuit between Terminal A and GND. I get the same result when the transceiver is completely off. By now I destroyed multiple transceivers with this setup.
If I ramp up with less than 1V/s the transceiver is not harmed. But this doens't seem to be the idea of the test nor the "Recommended Operation Conditions" given in the data sheet.
Can somebody tell me what I'm doing wrong or where it's specified that it's not possible to switch "fast" from 0V to -7V in the data sheet?
In case it's not possible, how can this transceiver comply with TIA-485-A?
Regards,
Raphael