This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: behavior when attached USB-C charger w/ PPS PDO

Part Number: TPS65982


Hi, everyone,

 TPS65982 doesn't support PPS (PD 3.0).

Is my understainding right?

When we attach Goppa ATREG27W_03 to our prducts using TPS56982, 

TPS65982 requests PPS (3.3V-11V Max. 3A), and repeats hard reset.

On the other hands, when we attach Aukey PA-Y10,

TPS65982 requests fixed PDO (20V Max. 2.3A) correctly,

except PPS (3V-16V Max. 3A).

Best Regards,