Part Number: TUSB2046B
Other Parts Discussed in Thread: TPS2042
Hello E2E community,
I used TUSB2046 to design a hub with one upstream port (USB type B), 2 downstream port (USB type A), and one port connected to an MCU. When I plug the upstream port to a PC, I get an error message “Unknown USB Device needs more power than the port can supply”. There are no devices connected to the down stream ports, but port 3 of the hub chip is connected to the MCU. I have done some troubleshooting and this is what I found:
PWRON1 & PWRON2 (pins 9 & 13) are both high (this disables the power-distribution switches TPS2042) although OVRCUR1 & OVRCUR2 are both high (no over-current condition)
I realised that we don't have 15k pulldown on DM3 DP3 lines, could this cause Power-Surge Error and deactivate all ports?
We left the unused OVRCUR3 & OVRCUR4 open, should they be pulled high?
Is there any error in this design?
Thank you for your help!