Part Number: TPS65987D
Hi, everyone,
Could you tell us the register settings to use "UCSI - SET_UOR" commands ?
for example:
[0x29 Port Control Register]
Bits 12: ProcessSwapToUFP should be 1.
Bits 14: ProcessSwapToDFP should be 1.
etc...
Our base firmware version is "F707.10.06",
and we've noticed SET_UOR commands won't work properly.
In our firmware setting, 0x29 Bits 12 ProcessSwapToUFP is set 0,
but if we set it 1,
we can issue SET_UOR command.
Best Regards,