Other Parts Discussed in Thread: TCAN1042-Q1
Hi team,
My customer is asking for TI CAN Transceiver solution. May I have your help for suggestion?
Thanks a lot for great support!
- The CAN pins shall operate to specification after exposure to voltages up to 30 V.
- [Note]: Nominal operating voltage is 24 V ± 1 V, Over-Voltage Protection is 27 to 30 V.
- The CAN Bus shall recover without intervention by an operator when ESD is applied to the outer metal shell
- [Note]: ESD SPEC as IEC 60601-1-2:2014: ± 8 kV contact, ± 15 kV air Horizontal/Vertical coupling plane the PSU shall recover without intervention by an operator.
Thanks a lot!
Sean Liao