Part Number: TPS65987DDJ
Dears
We want to adopt TPS65987DDJ in the design of Tablet product. Does this PD controller support QC 4.0? Or we need to add an external device to communicate with the HOST first?
Thanks
BR
Edward
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65987DDJ
Dears
We want to adopt TPS65987DDJ in the design of Tablet product. Does this PD controller support QC 4.0? Or we need to add an external device to communicate with the HOST first?
Thanks
BR
Edward
Hello Edward,
No, the TPS65987DDJ does not support Qualcomm charging. However, we are able to support PPS sink, which is only compatible with QC 4.0 source devises or devises that can support PPS source.