Part Number: THVD1500
Dear TI Experts,
May I know the EMI performance of THVD1500? and which IEC standard followed during the EMI test? Thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bruce,
THVD1500 bus pins reach these IEC standard (the tests follow the IEC standard).
– ± 8 kV IEC 61000-4-2 Contact Discharge
– ± 10 kV IEC 61000-4-2 Air Gap Discharge
– ± 2 kV IEC 61000-4-4 Fast Transient Burst.
What else are you interested? Please let me know if you have more questions.
Regards,
Hao