This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: programing alternatives

Part Number: TUSB9261


Hi,

I want to use the TUSB9261.  USB to SATA bridge. in my design

The design Host use USB 2.0

it exist system the Host and the device are connected (board to board).  the SATA device is removable.

Can I use USB 2.0 channel for programing the device? ( I read at the forms that someone had problems with that)

 the Host using Linux as OS, Can you provide programing tool that supported Linux ?

Can you recommended SPI flash for use with the TUSB9261 (data sheet include obsolete parts)

can I program SPI flash diractly ? how?

Thanks in advance

 Amir