Part Number: DP83640
Hi team,
My customer is curious about the PPS function. The output PPS signal is on the rising or falling edge corresponding to the whole second clock inside the PHY? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83640
Hi team,
My customer is curious about the PPS function. The output PPS signal is on the rising or falling edge corresponding to the whole second clock inside the PHY? Thanks.
Hi Lin,
How is this information going to be used in the application? Currently we do not specify if the PPS output is generate on rising or falling edge of the internal clock. However, this will be same for all DP83640 so that the PPS output will behave the same between device to device. The synchronization will not be affected.
-Regards
Aniruddha
Hi Charles,
The rising edge of the PPS output signal should be used as an indication that 1 second has passed. We recommend a similar strategy in our synchronization apo note: http://www.ti.com/lit/an/snoa548a/snoa548a.pdf
In the App note, the PHY relies on the PPS output of the GPS receiver and uses the rising edge. Same strategy can be used when PPS signal is generated as output of the PHY.
-Regards
Aniruddha