Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: DS90UB948-Q1
Hi team,
Can you answer the following questions of DS90UB947-Q1 and DS90UB948-Q1?
Case1: 1920 x 720, 95MHz
: Single Open-LDI (D0,1,2,3,CLK) -> DS90UB947-Q1 -> Signle FPD-LINK III -> DS90UB948-Q1 -> Dual Open-LDI output (47.5MHz per output)
-. Is the configuration available?
-. For unused pins (D4,5,6,7) of DS90UB947-Q1, should it be left as floating, or not?
-. For unused pins (RIN1) of DS90UB948-Q1, how should it handle?
Case2: 1920 x 720, 100MHz
: Single Open-LDI (D0,1,2,3,CLK) -> DS90UB947-Q1 -> Dual FPD-LINK III -> DS90UB948-Q1 -> Dual Open-LDI output (50MHz per output)
-. If LCD requires 50MHz, does above configuration have to be used?
Thanks,
Sam Lee