Part Number: DP83867IS
Hi everybody,
i am having issues by switching between 100 Mbps and 1000 Mbps modes. When auto-negotiation is enabled, the PHY is able to switch between 100 and 1000 but only if the PC side is limited to the specific data rate.
But i want to configure the PHY manually, so the PC builds up a 100 Mbps link when i configure the PHY in 100 Mbps mode. For that i turned in register 0x0000 bit 12 to "0" to disable auto-negotiation. Bits 6 (MSB) and 13 (LSB) turned to [01] for 100 Mbps and bit 8 to "1" for full duplex.
The RGMII side is running on 25 MHz but the ethernet side cant build up a link.
Many thanks for your help.