Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987, , TPS65988
Hi Team,
follow the PDF -- "TPS65987DDH Host Programming for SPI-Flash Less Systems" Application Report: SLVA972–May 2018;
we use a STM32F407 demo board as an external host, connect with TPS65987 over I2C.Our BusPowerZ Configurations is :
| BP_ECWait_internal | Infinite Wait |
We plug a PD charger type C,when power on, TPS65987 enter into PTCH mode, then STM32F407 will download the patch bundles to TPS65987, after download successfully, TPS65987 will reboot,and enter into PTCH mode again, that is not we wanted. Normally, it should enter into APP mode after download patch.
But if we plug a normal type C(just supply 5V), execute the above procedure, after download successfully, TPS65987 will not reboot , it can enter into APP mode, it is OK.
So what is the different ? How to make it work normally when plug a type C cable with PD charger?
Best Regards,
peng