Part Number: TUSB8041
Hi,
my customer wants to use usb8041 and has special requirements, he wants to implement a protection for the USB pins (USB_SSRXP etc) for lightning protection.
the max value at the pin is 1.4 V. DO I understand the parameter correctly, that is the value they would need to protect?
I found no TVS Diode in this range.
a TVS-Diode for USB3.0 would clamp at 2.1 V
Can you help?
Kind regards,
Marion