This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB544: TUSB544 EVM Question.

Part Number: TUSB544


Hi Sir,

Customer use TUSB544 EVM, there’s a problem that USB3 works but DP doesn’t work.

Would you pls help to check if something wrong for config?

Here is configuration:

SLP_S0# : High

VIO_SEL : 1k ohm to GND(Low)

I2C_EN : Floating

DIR1 : L

DIR0 : L

CTL1 : H

CTL0 : H

FLIP : L

SWAP : L

Thanks, Ian.