Part Number: DP83867IS
I'm using the TI PHY part DP83867IS on a Xilinx VCU118 development board. I switch to 6-wire mode and then perform the software workaround for the RX_CTRL strap (reg 0x31 bit 7 to 0). My FPGA receives the 625 MHz differential clock for 20 seconds and then the clock input to the FPGA for the MAC appears to stops. I've investigated the SGMII IP core in the FPGA and can't find any issues. I can still talk via MDIO to the TI PHY just fine after the timeout. If I power down and back up the TI PHY (via registers) or perform a software reset then the clock starts back up again for 20 seconds. It is very consistently 20 seconds. What could be causing this behavior? It almost seems like the TI part is in a sleep mode? Is it expecting certain responses from the MAC in order to provide the clock? Below is the MDIO register reads of the TI PHY and the Xilinx SGMII core - does anything jump out there? Thanks.
TI-PHY chip MDIO Read, PhyAddr: 3
------------------------------------------------------------
TI-PHY MDIO Addr: 0x000 0x00001140
TI-PHY MDIO Addr: 0x001 0x0000796d
TI-PHY MDIO Addr: 0x002 0x00002000
TI-PHY MDIO Addr: 0x003 0x0000a231
TI-PHY MDIO Addr: 0x004 0x000001e1
TI-PHY MDIO Addr: 0x005 0x0000cde1
TI-PHY MDIO Addr: 0x006 0x0000006d
TI-PHY MDIO Addr: 0x007 0x00002001
TI-PHY MDIO Addr: 0x008 0x00004006
TI-PHY MDIO Addr: 0x009 0x00000300
TI-PHY MDIO Addr: 0x00a 0x00003c00
TI-PHY MDIO Addr: 0x00b 0x00000000
TI-PHY MDIO Addr: 0x00c 0x00000000
TI-PHY MDIO Addr: 0x00d 0x0000401f
TI-PHY MDIO Addr: 0x00e 0x00000000
TI-PHY MDIO Addr: 0x00f 0x00003000
TI-PHY MDIO Addr: 0x010 0x00005841
TI-PHY MDIO Addr: 0x011 0x0000af02
TI-PHY MDIO Addr: 0x012 0x00000000
TI-PHY MDIO Addr: 0x013 0x00000000
TI-PHY MDIO Addr: 0x014 0x000029c7
TI-PHY MDIO Addr: 0x015 0x00000000
TI-PHY MDIO Addr: 0x016 0x00000000
TI-PHY MDIO Addr: 0x017 0x00000040
TI-PHY MDIO Addr: 0x018 0x00006150
TI-PHY MDIO Addr: 0x019 0x00004444
TI-PHY MDIO Addr: 0x01a 0x00000002
TI-PHY MDIO Addr: 0x01e 0x00000002
TI-PHY MDIO Addr: 0x01f 0x00000000
TI-PHY MDIO Addr: 0x025 0x00000400
TI-PHY MDIO Addr: 0x02d 0x00000000
TI-PHY MDIO Addr: 0x031 0x00001170
TI-PHY MDIO Addr: 0x032 0x00000000
TI-PHY MDIO Addr: 0x033 0x00000000
TI-PHY MDIO Addr: 0x037 0x00000000
TI-PHY MDIO Addr: 0x043 0x000007a0
TI-PHY MDIO Addr: 0x055 0x00000001
TI-PHY MDIO Addr: 0x06e 0x00000803
TI-PHY MDIO Addr: 0x06f 0x00000050
TI-PHY MDIO Addr: 0x0d3 0x00004000
TI-PHY MDIO Addr: 0x0dc 0x00003800
TI-PHY MDIO Addr: 0x0fe 0x0000e721
TI-PHY MDIO Addr: 0x134 0x00001000
TI-PHY MDIO Addr: 0x135 0x00000000
TI-PHY MDIO Addr: 0x170 0x00000c0f
TI-PHY MDIO Addr: 0x172 0x00000000
SGMII Core MDIO Read, PhyAddr: 5
------------------------------------------------------------
SGMII MDIO Addr: 0x00 0x00001140
SGMII MDIO Addr: 0x01 0x000001c8
SGMII MDIO Addr: 0x02 0x00000174
SGMII MDIO Addr: 0x03 0x00000c00
SGMII MDIO Addr: 0x04 0x00000001
SGMII MDIO Addr: 0x05 0x0000d801
SGMII MDIO Addr: 0x06 0x00000004
SGMII MDIO Addr: 0x07 0x00000000
SGMII MDIO Addr: 0x08 0x00000000
SGMII MDIO Addr: 0x0f 0x00008000
SGMII MDIO Addr: 0x10 0x00000003
TI-PHY chip MDIO Read, PhyAddr: 3
------------------------------------------------------------
TI-PHY MDIO Addr: 0x000 0x00001140
TI-PHY MDIO Addr: 0x001 0x0000796d
TI-PHY MDIO Addr: 0x002 0x00002000
TI-PHY MDIO Addr: 0x003 0x0000a231
TI-PHY MDIO Addr: 0x004 0x000001e1
TI-PHY MDIO Addr: 0x005 0x0000cde1
TI-PHY MDIO Addr: 0x006 0x0000006d
TI-PHY MDIO Addr: 0x007 0x00002001
TI-PHY MDIO Addr: 0x008 0x00004006
TI-PHY MDIO Addr: 0x009 0x00000300
TI-PHY MDIO Addr: 0x00a 0x00003c00
TI-PHY MDIO Addr: 0x00b 0x00000000
TI-PHY MDIO Addr: 0x00c 0x00000000
TI-PHY MDIO Addr: 0x00d 0x0000401f
TI-PHY MDIO Addr: 0x00e 0x00000000
TI-PHY MDIO Addr: 0x00f 0x00003000
TI-PHY MDIO Addr: 0x010 0x00005841
TI-PHY MDIO Addr: 0x011 0x0000af02
TI-PHY MDIO Addr: 0x012 0x00000000
TI-PHY MDIO Addr: 0x013 0x00000000
TI-PHY MDIO Addr: 0x014 0x000029c7
TI-PHY MDIO Addr: 0x015 0x00000000
TI-PHY MDIO Addr: 0x016 0x00000000
TI-PHY MDIO Addr: 0x017 0x00000040
TI-PHY MDIO Addr: 0x018 0x00006150
TI-PHY MDIO Addr: 0x019 0x00004444
TI-PHY MDIO Addr: 0x01a 0x00000002
TI-PHY MDIO Addr: 0x01e 0x00000002
TI-PHY MDIO Addr: 0x01f 0x00000000
TI-PHY MDIO Addr: 0x025 0x00000400
TI-PHY MDIO Addr: 0x02d 0x00000000
TI-PHY MDIO Addr: 0x031 0x00001170
TI-PHY MDIO Addr: 0x032 0x00000000
TI-PHY MDIO Addr: 0x033 0x00000000
TI-PHY MDIO Addr: 0x037 0x00000000
TI-PHY MDIO Addr: 0x043 0x000007a0
TI-PHY MDIO Addr: 0x055 0x00000001
TI-PHY MDIO Addr: 0x06e 0x00000803
TI-PHY MDIO Addr: 0x06f 0x00000050
TI-PHY MDIO Addr: 0x0d3 0x00004000
TI-PHY MDIO Addr: 0x0dc 0x00003800
TI-PHY MDIO Addr: 0x0fe 0x0000e721
TI-PHY MDIO Addr: 0x134 0x00001000
TI-PHY MDIO Addr: 0x135 0x00000000
TI-PHY MDIO Addr: 0x170 0x00000c0f
TI-PHY MDIO Addr: 0x172 0x00000000
(SGMII clock to FPGA now stopped!)
SGMII Core MDIO Read, PhyAddr: 5
------------------------------------------------------------
SGMII MDIO Addr: 0x00 0x00000000
SGMII MDIO Addr: 0x01 0x00000000
SGMII MDIO Addr: 0x02 0x00000000
SGMII MDIO Addr: 0x03 0x00000000
SGMII MDIO Addr: 0x04 0x00000000
SGMII MDIO Addr: 0x05 0x00000000
SGMII MDIO Addr: 0x06 0x00000000
SGMII MDIO Addr: 0x07 0x00000000
SGMII MDIO Addr: 0x08 0x00000000
SGMII MDIO Addr: 0x0f 0x00000000
SGMII MDIO Addr: 0x10 0x00000000