This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD3088E: Capacitative loading of cable side I/O pins (A and B).

Part Number: SN65HVD3088E


In order to filter the received signals at the SN65HVD3088E, I have shunted the A and B pins with 100pF capacitors to ground.

Is this acceptable, the data sheet doesn't explicitly say.

  • Hi Robert,

    Yes, this is acceptable.  RS-485 networks are often subject to much higher capacitive loading due to the parasitic capacitance of the cabling used, which can be quite long.  At a certain point the low-pass effect will limit the bandwidth of the transmission line (and therefore limit the maximum data rate achievable), but I wouldn't expect 100 pF to cause much degradation.  You can check the A/B signal waveforms to make sure they aren't "rolled off" too much and are able to reach their full-scale amplitudes within a reasonable time to verify there are no issues in this application.

    Regards,
    Max