Part Number: DP83640
Hi Champs,
I have some TI EVMs using this PHY and the source code tried to access a PHY register called PHY_LINK_PARTNER_SPD via MDIO read. In older code: the PHY_LINK_PARTNER_SPD is defined as offset 10u. However, newer code this is defined as 16u.
I looked at http://www.ti.com/lit/ds/symlink/dp83640.pdf, Table 5-9. Register Map
- 08h-0Fh 8-15 RESERVED RESERVED
- 10h 16 RO PHYSTS PHY Status Register
It looks that 10u is reserved and 16u is PHY status.
Q1. Can you clarify the correct offset of this PHY_LINK_PARTNER_SPD?
Q2. Can you give the bit level explanation of the register? E.g, how do I interpret the readback value?
Regards, Eric