Part Number: SCAN921226H
What dose this 27ohm load mean?
Can you please explain the difference between the 27ohm load and the 100ohm terminal resistance? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SCAN921226H
What dose this 27ohm load mean?
Can you please explain the difference between the 27ohm load and the 100ohm terminal resistance? Thanks.
Daniel
Bus LVDS drives multi-drop or multi-point application. While the typical termination impedance is 100 ohm, but with multiple drivers or receivers, the additional loading due to these extra driver/receivers will result in an effective impedance of considerably less than 100 ohm.
Thanks
David
Thanks for your info.
If the Bus LVDS drives point-point application, the typical termination impedance should be 100 ohm and the typical differential voltage should be 350 mV, right?
Can you answer me another question? I want to put a common mode choke on the lvds data lines. How does the differential mode impedance of the choke affect the differential voltage margin of the receiving end? Should I do a voltage divider to calculate the margin? Thanks.
Daniel
For point-point application, the typical termination impedance is 100ohm and differential voltage swing of 350mV.
For calculate the margin, it is better to run a simulation to calculate the differential voltage margin since the amount of margin also depends on the data rate, cable insertion loss, etc.
Thanks
David