Hi,team
I am using DS90UB960+DS90UB935. I have config 960 and 935 to CSI2 sync mode by idx pin. And set 960's register 0x58 to 0x5e. But the 960's register 0x5B always 0x00.
Already checked the power supply,look all fine. Any idea can help me ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,team
I am using DS90UB960+DS90UB935. I have config 960 and 935 to CSI2 sync mode by idx pin. And set 960's register 0x58 to 0x5e. But the 960's register 0x5B always 0x00.
Already checked the power supply,look all fine. Any idea can help me ?
Hello Xuhui,
Is the 935 also pin strapped for synchronous mode?
Thanks,
Casey
Hi, Casey,
935 alreay in synchronous mode, Mode pin's R high is NC, R low is 10k. But 960's sync mode called csi2 mode,it that right?
Hello
Can you ensure that 960 is linked up first? Do you see stable lock on the channel you connected to 935?
Thanks
Vijay
Hi Vijay,
There is no lock state show in 960's registers, and 0x5b register always 0x00.
BTW,i already can use 960+913 get frames. For 960+935, i only change the mode pin to csi mode.
Thanks
Xuhui
Hello Xuhui
Looks like the receiver is not locked and that's the reason you dont have remote i2c access. LOCK status can be read from register 0x4D available on the 960
Thanks
Vijay
Hi,Vijay
I solved it, my pcb layout has some issure. Thank you very much.
And i want communicate with camera sensor via i2c, which register i need config? 0x5d SlaveID or 0x65 SlaveAlias ??
Xuhui
If you only have 1 imager, use slaveID. If you have multiple imagers with same i2c address, u can use aliasing to address the cameras
Thanks
Vijay