Part Number: TUSB8040A1
Hi,
I am using several TUSB8040A1 in my design, the connection is as follows:
One main TUSB8040A1 and two additional TUSB8040A1 the are connected to ports 0 and 3 on the root HUB.
When a board is connected to PC, devices are recognized as connected to ports 3 and 0.
On one of the boards, the devices are recognized as connected to ports 3 and 2.
What can be the issue? is there any internal EEPROM that can be corrupted?