Part Number: SN75DP130
Hello,
We use the P/N SN75DP130DSRGZT (dual-supply) as a source re-driver. We do not do anything special with setting, all register values are default programming. The issue we have is that we can drive only some Dell monitors but not every Dell monitor we are able to find in our lab. Test set-up: 1080p60 output using a 6-ft long DP cable to 5 different Dell monitors with DP port, 3 models work OK and 2 not working, ie nothing shown on the screen and monitor go eventually to sleep mode). We keep the set-up identical and just swap Dell monitor.
Note: all Dell monitors work OK with different DP sources or PC and unfortunately we can find only one sample of each Dell monitor in the lab.
Note: also, when it work or does not work, the result is consistent on multiple attempts
Since we set CAD_SNK pin = 0 (DP sink), I assume the link training is monitored by the DP130 and it sets automatically output swing, pre-emphasis gain and equalization gain according to training info. What else can we do better if we choose to do manually?
If it is signal integrity, what can we improve on re-driver side?
Thanks
Lam Huynh