Hi,
we are designing a simple full speed USB device with USB type C connectorthat will connect to tablet/phone and jack/another USB type C connector for external power supply/adapter. There will be 2 power modes of the system:
1) No external power supply connected to the device - then the tablet must supply power for the device.
2) External power supply connected to the device - then the device supplies power on the bus and the tablet/phone can charge itself.
It can be switched between 1) and 2) during runtime (when external power supply is connected/disconnected).
Can you please recommend suitable controller IC for this?