Hi
I have my TPS65987EVM here and am trying to get it to work with the application customization tool.
I am running Win 10 and my laptop only has USBC ports, so I am connecting the micro USB connector U3 via a USBC converter. In device manager I can see USB Serial Converter A, B, C, and D.
When I try the test read on the import configuration from device dialog I get the following exception:
Exception Encountered during I2C Test Read:*** ERROR in FTDI call (I2C_DeviceWrite), status: 2
<type 'exceptions.Exception'>
Traceback (most recent call last):
File "dialogWindow.pyc", line 3143, in test_read
File "device_rw.pyc", line 174, in read_reg
File "hw_interface.pyc", line 405, in hw_i2c_write_no_stop
File "ftdi.pyc", line 314, in ftdi_i2c_write
Exception
I have tried installing the 3 different FTDI drivers that come with the download pack and I downloaded the software tool today. Version is 5.1.
Do you have any ideas?
Also, I have power going to the board via a wire I soldered onto the back of the DC jack connector. Could you point me in the direction of a recommended plug connector part number? The BOM lists the Foxconn connector but they have no information for a mating plug.
Thanks