Part Number: HD3SS3220
Our current Design has the HD3SS3220 in an UPF configuration like in the data sheet and is connected to a hub. Power and USB 2 is working but not getting any USB 3. When I looked at the LFPS polling signal at the connector it is biased around ground wich I don't think is correct. I looked at the signal going into the Hub and it is biased around ground also. I do not ave any capacitors on RX1 and RX2 pairs as the data sheet shows nor do I have any on the RX pairs going to the HUB. Is the lack of caps in the RX path causing the bias problem? Do I need to add caps either to the RX1 and RX2 pairs or do I just need to add caps in RX pair to the HUB?
Tony Carter