This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK2711-SP: package dimensions & material

Part Number: TLK2711-SP

Could you let me know the package information as follows?

P/N:
5962-0522101VXC

・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au

・Lid material/ base plating /plating (ex. Covar/Ni/Au

・Package cavity wall thickness(mm) (ex. 0.25mm

・Lid thickness(mm) (ex. 0.25mm

・Part weight(typ. grams) (ex. 3.5g

・Part weight(max. grams) (ex. 4.0g


We'd like to use it for a thermal & radiation analysis.


Regards,
Tom4073.cavity wall and lid definition.pdf

  • Tom,

    Please give us a few days to research and align on answer.

    Thanks,

    Wade

  • Tom,

    I will need a little more time to locate one last piece of information on this device. 

    The other devices requested should be forthcoming shortly.

    Regards,

    Wade

  • Here are the values.  Please note that these are typical values.

    5962-0522101VXC

    ・Package material/ base plating /plating  : Alumina/Ni/Au

    ・Lid material/ base plating /plating:  Kovar/Ni/Au

    ・Package cavity wall thickness(mm)    3.62,3.62 ( x,  y dimensions)  Note, that the package cavity has 2 tiers.  The value provided is for the widest tier, with the thinnest cavity wall.

    ・Lid thickness(mm) 0.25

    ・Part weight(typ. grams) 4.5 : Note, this includes the entire package with the tie bar.   I do not have good data on mass of the tie bars, but they are estimated to be approximately 1gram based on the mass of similar HFG package tie bar.

    If this answers your question, please click "This Resolved My Issue"
    Regards,
    Wade