This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: can 960 support receive 36 frames/second images of three cameras?

Part Number: DS90UB960-Q1


Hi team,

1.DS90UB960-Q1, Four channels 1080p@30fps when connected to the loop view. If the device switching mode only requires three cameras to work, can DS90UB960-Q1 only receive 36 frames/second images of three cameras?

That is, if you don't need a camera, close the DS90UB960-Q1 channel instead of filling the "0" data with the camera.

2. LCD display serializer: Is there a single coaxial transmission 4-channel 1080p@30fps serializer?

Thanks

Gene

  • Hello Gene,

    1. Yes, you can disable an RX port to reduce the camera bandwidth input to 960

    2. Are you asking if there is a serializer which can take in four independant camera inputs? Or are you asking if the output of 960 can be fed into a serializer with 4 streams on virtual channels?

    Best Regards,

    Casey