Part Number: TL16C754C
The pin table on datasheet doesn't show the RXRDY/TXRDY pin No. for TL16CP754C.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TL16C754C
The pin table on datasheet doesn't show the RXRDY/TXRDY pin No. for TL16CP754C.
Hey Stephen,
I was able to look at the older datasheet and it seems we used to have an 80 pin version of this device which had the RXRDY and TXRDY pins. At some point, the 80 pin device was removed and only this version of the device remained, which the 64 pin version we have no longer has the RXRDY/TXRDY pins. I looked at a mount bond diagram internally and saw that there were two pads on the die which were not connected to the leadframe, this indicates to me that those unconnected pads were the RXRDY and TXRDY pins of this device.
On my part, it looks like I will need to modify this datasheet to remove mention of TXRDY/RXRDY and to make it clear the TL16CP and TL16C do not have RXRDY and TXRDY.
Thanks,
-Bobby