This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP130SSEVM: Interface forum

Part Number: DP130SSEVM
Other Parts Discussed in Thread: TDP142

Dear TI Team,

i'd like to use the DP130 in a sink application with a DP to VGA converter,Could it work?

1. Is it possible to get the evaluation board manual, schematics and other relevant design files as a reference?

2. Regarding link training:  For a sink application the automatic link training needs to be switched off to set fixed levels/values for the DP130 output lanes. These should be configured by I2C. Will it also be necessary to implement the link training for clock and EQ on the input via I2C ? Or will this still work automatically? If not: Would be sufficient to use a external controller that polls the I2C registers ?

Best regards,

yangguangzheng