Part Number: SN65DP159
Other Parts Discussed in Thread: DP159RSBEVM, TMDS181
Hello,
I would like to ask a question for SN65DP159.
I am currently using SN65DP159 on HDMI input port.
The schematic is similar to the DP159RSBEVM.
- TMDS Termination resistances are located near HDMI CN. (50ohm pull-up on each TMDS line)
- AC Caps are used between HDMI CN and SN65DP159.
In this case, we checked the Hot-TDR but the average value were approximately 50 ohm.(Failed)
Then, I took off the AC caps as a experiment.
It means that TMDS lines are not connected from HDMI CN to SN65DP159.
But the Hot-TDR value were improved to approximately 100ohm.
Here is my question.
To compliant with Hot-TDR requirement for HDMI2.0 sink by using SN65DP159,
what should we improve for it? Do you have any idea?
Or, should we change the SN65DP159 to TMDS181?
I would appreciate it if you could give me some suggestion.
Best regards,