Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65988
Hi,
I would have several questions regarding this device
- would this one, The -DJ variant or the TPS65988 be released also in industrial spec (-40 to 125 degree C) if yes, when?
you can provide this information privately as well
- Is there a roadmap/ new developments? -> also in private maybe provided
- Can this device family also work with 3rd party Power converters (I2C feedback)
- Can you recommend the newest Buck-Boost, that would work with those devices?
- If you use TUSB1046A with it, :
- are the EQ values fix?
- with debugging, do you need to load the firmware everytime if you want to change the EQ values?
Thank you for your help,
kind regards,
Marion