This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD3S716-Q1: devices protections when unpowered

Part Number: TPD3S716-Q1


Hello,

I am planning to use the TPD3S716-Q1 for USB interface protection in a USB 2.0 OTG application. Since this is USB OTG, it is possible that someone will plug in a USB device that supplies 5V while my board is unpowered. If this happens, will the TPD3S716-Q1 prevent any current from leaking into the rest of my circuit? In this situation, VBUS_CONN will be at 5V, VD+ and VD- may be at 3.3V, VBUS_SYS will be at 0V, VIN will be at 0V, and all other pins will be at 0V. 

Additionally, in this scenario, will the TPD3S716-Q1 still provide overvoltage and ESD protection? What about any other protections?

Thanks