For customer's request, I would like to know simple I2C swtihcing device with 4 channel.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mark,
Can you clarify what you mean by 4 channel? Is it Configuration (1:4) or (4:1) or Number of Channels (4)?
We have some good recommendations for 1:4 configuration switching devices that support I2C signals:
1: The TMUX1209 is one of our new devices. It is a 2-ch, 4:1 Mux that has 1.8-V compatible control inputs. with 42 pF (typ) CON
2: If you are looking for lower CON, SN74LV4052A is a good option It is a Dual 4-channel analog multiplexer and demultiplexer with CON of 5.6pF (Typ).
Based on your requirements, you can select from the above options.
Please let me know if you have further questions.
Thanks
Saminah