Part Number: TCAN334
1.What should the capacity of "CSPLIT" be when the termination method is "Split Termination"?
2.What is "integrated pull down"?
Is it necessary to pull down SHDN and STB externally?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN334
1.What should the capacity of "CSPLIT" be when the termination method is "Split Termination"?
2.What is "integrated pull down"?
Is it necessary to pull down SHDN and STB externally?
Hello,
For CSPLIT, an exact value is not required but a common recommendation is 4.7 nF. This capacitance is intended to provide a low-impedance path to ground for high-frequency common mode noise, and changing the capacitance value would vary the range over which the filtering would be effective.
If a logic input has an integrated pull-down, it means that if nothing else drives a voltage onto the input then its state will be biased to a low level. This is equivalent in function to an external pull-down resistance. However, in the case of the SHDN and STB pins the internal pull-down function is very weak. To avoid things like leakage currents or coupled noise from unintentionally toggling these pins, I would recommend using an additional external pull-down resistor (valued between 1 kOhm and 10 kOhm) on these pins if they will be high-impedance in the application.
Please let me know if this is unclear or if you have any further questions.
Regards,
Max