Part Number: DS90UR910QEVM
Other Parts Discussed in Thread: ALP, USB2ANY
Hi,
I am evaluating DS90UR910QEVM.
Serializer is DS90UR241Q and Deserializer is DS90UR910QEVM.
LVDS link is up and runs fine. I see pass and lock indicator is constantly ON.
The only trouble that I am getting right now is programming
No response over I2C protocol. Connections are right, conversion works, but no response over I2C communication. Tried several I2C masters but simply SDA/SCL remains always high.
Tried multiple I2C platforms Android, Linux, Windows - multiple I2C devices but simply both SDA/SCL is always high and No response from the slave.
Tried all possible variation for the I2C slave address but no response.
PDN is high, BIST is low, S2 all low, ID1,ID0 tried all combination, Config 1 High, Config 0 Low for DS90UR241Q.
Pull up resistor values are nominal.
The only modification done to EVM is populating C18, C17.
Any help would be appreciated.