Part Number: SN65176B
Other Parts Discussed in Thread: THVD1500, THVD1550
I want to keep this device active.
Is it safe to always connect VCC(5v) to the DE pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Akaba-san,
Yes, there is no issue for the SN65176B when tying DE to VCC (5 V). However, this should only be done if your application involves simplex (uni-directional) data transfer. If the SN65176B will need to receive data from other nodes (or if the other nodes need to communicate data via the RS-485 bus at any time), you would need some mechanism to disable the driver output so that the SN65175B output does not interfere with the outputs of other nodes.
Please let me know if this is unclear or if you have any further questions.
By the way, SN65176B is a fairly old device. For new designs you may want to consider more modern transceivers such as THVD1500 (for data rates up to 500 kbps) or THVD1550 (for data rates up to 50 Mbps). These devices are pin-for-pin compatible but have a number of improvements such as enhanced ESD/noise immunity, wider supply voltage tolerance, support for higher node counts, and integrated failsafe biasing.
Regards,
Max Robertson