Part Number: TCA9555
Other Parts Discussed in Thread: STRIKE
Team,
There are a few tables and descriptions concerning the internal POR and glitches, could you provide further information or guidance concerning the following questions?
- Page 29/30 of the PDF of the datasheet http://www.ti.com/lit/ds/symlink/tca9555.pdf says that glitches in the power supply can also affect the power-on reset performance of this device. Can you comment on the state of the outputs of the device assuming that the device experiences a glitch that is considered in the functional disruption range?
- Page 16, 9.4.1 describes the power-on sequence of the device holding the outputs in a reset state.
- Are all output states held until the device’s VPROF threshold is met during power ramp-down?
- What happens to the output states between VPROF and 0V during the power-down?
- What happens to the output states if a glitch is encountered (described in question 1) during 2.a, between VCC and VPROF?
- What happens to the output states if a glitch is encountered (described in question 1) during 2.b, between VPROF and GND?
- Is there any condition other than a power glitch described on pages 29 and 30, that would result in unknown output states of the device?
- The default state of these I/O appear to be inputs. Is the 100K Ohm resistor on Page 17 present during power-up?
- Does the device have to receive valid commands prior to being configured for outputting on each port?
- Once default states are established, if a power glitch occurs, will the outputs return to the default states, or be reconfigured as inputs, or does it depend on the type of glitch that may have occurred?
- During a ramp-down with no power-down sequence glitch, do the I/O transition from the configured output --> to the default state defined --> input with 100K --> and finally no-operational?
Thank you.