Part Number: TS3DV421
can these parts be used for switching 100R diff pairs.
these wouldn’t be logic signals as per device intention, rather 100R differential baseband analogue signals, detail below:
100R diff pair analogue
Bandwidth: DC to 100MHz
Common mode voltage: 1V
Differential Vp-p: 600mV
I am assuming that all 4 channels have the same switch topology, and this is simply FET switches, so should handle analogue signals OK?
What would be the best supply rail setup to use with the device for my application, as I notice there are options?
Would you recommend any other options perhaps?