Part Number: DP83867IS
DP83867ISRGZ Device VDDIO are set to 1.8V and captured the waveform are at the pins 32, 33, 34,35 & 36. Observed that waveform are having more ringing and VOL seems shifted to around 0.5V. But, As per the datasheet VOL should be 0.2V only. Please refer the attached waveform.
Please help us to get proper waveform and is there any way to increase the RX signal drive strength.