This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL16C752D: The difference of FCR[7:6] between TL16C752D and TL16C752B

Part Number: TL16C752D

Hello,

Could you tell me why the FCR [7: 6] value has changed between TL16C752B and TL16C752D?

<TL16C752B>

<TL16C752D>

Best Regards,

Kaede Kudo

  • Hello Kudo-san,

    I don't have the history to know why the change was made for this specific product family, but I can tell you in general that it is beneficial to have some options available for lower trigger thresholds.  In the case of an application that only sporadically receives data, this allows the processor to detect the word reception sooner (rather than waiting for the FIFO to accumulate more data or for a timeout to occur).

    Regards,
    Max Robertson

  • Hello Robertson-san,

    Thank you for your answer.
    I understood it.

    It's just a confirmation, but it's not a typo.

    Best Regards,

    Kudo